Technical FAQs

Ask a Question

In ATV66 I have found the following programing. By Pass: YES Start Input: LI4 CD contact output: R2 Delay Time: 0,2 Sequence Tof: 5 Proccess Tof: 60 W...

Goals and Symptoms

In ATV66 I have found the following programing. By Pass: YES Start Input: LI4 CD contact output: R2 Delay Time: 0,2 Sequence Tof: 5 Proccess Tof: 60 We will supply him with an ATV58.Is the programming above relative with the "downstream contactor control" with R2 relay in ATV58.And if it is not, what must we program in ATV58 to have the same result

Causes and Fixes

The Bypass is equal to downstream contactor but is not possible to adjust the temporisation, if you need this function , please use ATV68.


Legacy KB System (APS) Data: RESL157589 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 66
Was this helpful?
What can we do to improve the information ?