Technical FAQs

Ask a Question

Do our ATV58ED16N4 and ATV58ED33N4 comply with (1) Zone 2 (2) Gas group IIA (3) Temp. Class T3 We need this i...

Goals and Symptoms

Do our ATV58ED16N4 and ATV58ED33N4 comply with
(1) Zone 2
(2) Gas group IIA
(3) Temp. Class T3

We need this information since this is needed for Oil & Gas Company.

Facts and Changes

ATV58ED

Causes and Fixes

As I can see your request concern explosive ambiance, our ATV don't respond to that, you need a special enclosure.


Legacy KB System (APS) Data: RESL157588 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?