Technical FAQs

Ask a Question

Can we use (connect to ATV68) communication cards (Modbus RTU card) and Programming terminal remote mounting kit VW3A68800 at the same time?

Goals and Symptoms

Can we use (connect to ATV68) communication cards (Modbus RTU card) and Programming terminal remote mounting kit VW3A68800 at the same time?

Facts and Changes

Modbus card VW3A68800

Causes and Fixes

It's not possible to use the both in the same time.


Legacy KB System (APS) Data: RESL157577 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 68
Was this helpful?
What can we do to improve the information ?