Technical FAQs

Ask a Question

XBTG: Popup windows note :movement and size

Popup window note
1- you can display up to 3 popup windows at one time.
Once the limit is reached, a popup window must be closed before you can open a new one.

2- The XBTG series support a movement in 8 pixels intervals. If you define a move of 7 pixels, there is no movement.

3- The XBTG series support width in multiple 8 pixels.
If you define the witdth of 1-7 pixels multiple, the windows width is changed by X-position.


Legacy KB System (APS) Data: RESL157550 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT-F, TXBT-F
Was this helpful?
What can we do to improve the information ?