Technical FAQs

Ask a Question

What cycle times are used for fields on application/alarm pages of XBT operator panels? Are these the same as for the dialogue table? What if you don'...

Goals and Symptoms

What cycle times are used for fields on application/alarm pages of XBT operator panels? Are these the same as for the dialogue table? What if you don't use the dialogue table?

Facts and Changes

XBTHM

Causes and Fixes

The communication is sampled at 400ms. The dialog table has priority. The requests to refresh variables are sent once the dialog table is over. In the case of the cycle time of the dialog table is under 400ms, only a few requests will have time to be sent between the dialog table. So, in case of a high number of variables to refresh, it is recommanded to set the cycle time of the dialog table > to 400ms to let time to send the requests.
The exchange principle also depends on the protocol chosen according to the type of PLC, and the category of variables to be displayed.
The XBT optimizes the refresh of variables by categories:
Types of variables: Word, doubleword, bit,...
Under types: Word bit, input bit, ...
EQUIPMENTs: Master, PLC, ...
Group: Init variables group (min, max), Cyclic variables group (Read or Read-Write refreshing fields)
Priority: Normal (variable in application page), Fast (Dialog table variable).
To summarize:
In order to optimize the refreshing of variables, when building a page, by category, the variables adresses should be consecutive.
 


Legacy KB System (APS) Data: RESL157532 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT -H, XBT-P, XBT-E
Was this helpful?
What can we do to improve the information ?