Technical FAQs

Ask a Question

Unable to Close ATV58HD33N4 Front Door when using Fipio card with TSXFPACC12 Connector

Goals and Symptoms

When using the VW3A58301 Fipio Card with a ATV58HD33N4, it states in the manual to use a TSXFPACC12 connector. The problem i have is when using this connector the cables are on the right hand side. When connecting to the Fipio card in the ATV58HD33N4, i am unable to close the front door. Please advise.

Facts and Changes


Causes and Fixes

Due to a design incompatibility, the solution is to not use the ACC12 connector. It is not possible to modify the product.

Legacy KB System (APS) Data: RESL157395 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?