Technical FAQs

Ask a Question

Importing Concept project does not contain Profibus information .

Go to the Parameters button of the Profibus I/O module in the I/O map and make sure 'Add upload info' is set.


Legacy KB System (APS) Data: RESL157384 V1.0, Originally authored by DaSo on 12/12/2012, Last Edited by DaSo on 12/12/2012
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?