Technical FAQs

Ask a Question

I need a diagram or description of the wire connections inside the cable supplied with the ATS48 remote terminal, part number VW3 G48101. I also need...

Goals and Symptoms

I need a diagram or description of the wire connections inside the cable supplied with the ATS48 remote terminal, part number VW3 G48101. I also need the part number for only the ATS48 remote keypad.

Facts and Changes

I have a good ATS48 customer who cannot read the ATS48 red LED keypad when it is exposed to bright sunshine (which is very common in his applications). He has good ATS48 control boards, but they are not bright enough. He can continue to use the ATS48 if he can buy only the remote keypad and make his own cable.

Causes and Fixes

The symbol of the keypad is W814943540111 and you can order it by SPEED.

For the cable, the wiring is:

RJ45: SubD 9 pins

4 - DB 3 - DA
5 - DA 4 - 0v
7 - 10v 6 - 10v
8 - 0v 7 - DB


Legacy KB System (APS) Data: RESL157343 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altistart 48
Was this helpful?
What can we do to improve the information ?