Technical FAQs

Ask a Question

ATV38 RFI Filter. Value of leakage current for size > 15 kW

Goals and Symptoms

ATV38
RFI Filter.
Value of leakage current for size > 15 kW

Causes and Fixes

It's the same filters like ATV68. The values are in VVD Catalog ( Dec 2002 ) page 2/236


Legacy KB System (APS) Data: RESL157278 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38
Was this helpful?
What can we do to improve the information ?