Technical FAQs

Ask a Question

Can the 170ENT11001 be used as a replacement for the 170ENT11000?

Yes, the 170ENT11001 can be used as a replacement for the 170ENT11000 however, the set up and configuration of the IP address and communication is quite different. The 170ENT11001 is a 10/100 base-T Ethernet with auto sensing and detection. This Module also supports FDR (Faulty Device Replacement). You must download the user manual for the 170ENT11001 in order to learn how to work with this new module. Many of the configuration steps have changed.


Legacy KB System (APS) Data: RESL157269 V1.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?