Technical FAQs

Ask a Question

How is a normal thermistor's resistance value that will not cause ATV68 tripped? What is the minimum thermistor's resistance value caused ATV68 tripp...

Goals and Symptoms

How is a normal thermistor's resistance value that will not cause ATV68 tripped? What is the minimum thermistor's resistance value caused ATV68 tripped?

Causes and Fixes

This information is available in the User's manual:
nominal value: < 1,5 kOhms
Tripping: 3 kOhms
Reinitialization: 1,8 kOhms

Was this helpful?
What can we do to improve the information ?