Technical FAQs

Ask a Question

analog output - want to use rectangle wave to match with existed customer's control board. Our customer has a board to check frequency signal but it's...

Goals and Symptoms

analog output - want to use rectangle wave to match with existed customer's control board. Our customer has a board to check frequency signal but it's only consider rectangle pulse counting which has same amplitude (10V Amplitude) for various frequency signal, and it's changed only rectangle pulse width. Is there any way to meet this application ?

Facts and Changes

atv 11 analog output

Causes and Fixes

It's a PWM and the range for cyclic report is 0 for 0% of the analog value, 100 for 100 % of the analog value.


Legacy KB System (APS) Data: RESL157240 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 11
Was this helpful?
What can we do to improve the information ?