Technical FAQs

Ask a Question

We are op against Omron 3G3F in a application which demands very high acceleration and deceleration, do to that we needs very short torque response ti...

Goals and Symptoms

We are op against Omron 3G3F in a application which demands very high acceleration and deceleration, do to that we needs very short torque response time and high bandwidth. Omron has, do to there manual, a band wide of 40 Hz, can ATV58F do that better.?

Causes and Fixes

The bandwidth for the 58F is about 20 Hz ( close loop )


Legacy KB System (APS) Data: RESL157203 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?