Technical FAQs

Ask a Question

Can we use ATV58 in ENA system for sucker rod pump as in ATV66 ? and what in the normal settings in this case ? for ATV68 what is the required setting...

Goals and Symptoms

Can we use ATV58 in ENA system for sucker rod pump as in ATV66 ? and what in the normal settings in this case ? for ATV68 what is the required settings ?

Causes and Fixes

Not possible with ATV58 but available with ATV68 under PSR6 software version.


Legacy KB System (APS) Data: RESL157198 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 28
Was this helpful?
What can we do to improve the information ?