Technical FAQs

Ask a Question

How many Remote Modbus Plus clients can be connected to one Modbus Plus host interface Server card?

You can have as many clients pointing to any one server as you like. The limitation is the Modbus Plus interface card itself. The card can handle 8 data master paths, 8 data slave paths, 8 programming paths and 8 programming slave paths. As long as these limitations are not exceeded the remote clients will be able to use the remote server as a connection to the Modbus Plus network over ethernet.


Was this helpful?
What can we do to improve the information ?