Technical FAQs

Ask a Question

Does the NW-BP85-002 require any programming in order to commission the unit?

No. The BP85 does not require any programming. All the user has to do to commission the unit is to set the MB+ address dip switches for both networks and power up the unit.

Was this helpful?
What can we do to improve the information ?