Technical FAQs

Ask a Question

WHY IS NOT POSSIBLE TO RUN OR STOP VIA POWERSUITE OR TERMINAL? I CONECT ON LINE POWERSUITE V1.5 TO ATV28 AND VISUALIZE STATE AND PARAMETERS VIA RADIO-...

Goals and Symptoms

WHY IS NOT POSSIBLE TO RUN OR STOP VIA POWERSUITE OR TERMINAL? I CONECT ON LINE POWERSUITE V1.5 TO ATV28 AND VISUALIZE STATE AND PARAMETERS VIA RADIO-MODEN BUT WHEN I RUN VIA POWERSUITE OR TERMINALS THE DRIVE AND ERROR MESSAGE APPEARS IN PC SCREEN: PARAMETER NOT KNOWN IN DATE BASE.

Facts and Changes

POWERSUITE CONECTED VIA RADIO-MODEN TO ATV28. TESTING WITH ATV58 NO PROBLEMS.

Causes and Fixes

1- Check the control mode: if the ATV28 is in local mode, it's not possible to drive it with the serial link.
2- Check the faults displayed by the radio-modem and by the ATV28 (it helps for the maintenance)
3- Check the Drivecom control register (address=W400).
4- Test the radio-modem emission and reception part far from the ATV28 because it could be perturbated with electromagnetic waves.
5- Check the model of the radio-modem and its communication characteristics.Then, adjust the communication parameters of the radio-modem or the ATV28.

Was this helpful?
What can we do to improve the information ?