Technical FAQs

Ask a Question

What are acceptable Impedance measurements for a Modbus Plus Network cable?

A properly installed Modbus Plus cable will have a measurement between 60 and 80 ohms. This measurement will be taken between pins 2 & 3 of the MB+ connector.
Improperly installed or defective cabling can have a measured value of 60 or 120 ohms.
For more information reference the Modbus Plus Planning and Installation Guide (P/N) 890 USE 100 00 for additional information.


Legacy KB System (APS) Data: RESL156824 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?