Technical FAQs

Ask a Question

What is the current draw on the XBT-N200 and XBT-N400?

The XBT-N200 and XBT-N400 get there power from the cable which is a 5v signal. The 5v signal is 1 watt, so the current draw is 200ma.


Legacy KB System (APS) Data: RESL156807 V1.0, Originally authored by on , Last Edited by on
Related ranges: XBT-K, XBT-B, XBT-A, XBT-V...
Was this helpful?
What can we do to improve the information ?