Technical FAQs

Ask a Question

What is the new F12 fault error on 5.51 Lexium firmware?

The F12 fault is used to detect whether the motor is connected to the drive power output. ( X9 connector).
To disable this feature, set the parameter CPHASE to zero.


Legacy KB System (APS) Data: RESL156769 V1.0, Originally authored by on , Last Edited by on
Related ranges: Lexium MHD
Was this helpful?
What can we do to improve the information ?