Technical FAQs

Ask a Question

A customer would like to use LONWORKS in order to link with ATV38. Does LONWORKS provide its network management in "Windows" version in order to perfo...

Goals and Symptoms

A customer would like to use LONWORKS in order to link with ATV38. Does LONWORKS provide its network management in "Windows" version in order to perform address assign, commissioning, network variable bindings and configuration? Does LONWORKS provide another modle as if those communication cards which can be mounted on ATV38's control board?

Causes and Fixes

For the management it depend to the used master, but now all software are under Windows, more informations at: www.lonworks.com or www.gongkong.com.
The parameter table for ATV58 is fixed in the gateway.

Was this helpful?
What can we do to improve the information ?