Technical FAQs

Ask a Question

Do the XMIT, 984 LL, and the XXMIT, IEC, support Modbus "Broadcast" mode?


Yes, the XMIT, 984 LL, and the XXMIT, IEC, support Modbus "Broadcast" mode. The "Broadcast" mode is only supported by the Modbus function codes that write to Modbus slaves. "Broadcast" mode is not supported by the Modbus function codes that read from Modbus slaves. A "Broadcast" is initiated when a value of zero, 0, is entered for the Modbus slave address.

Was this helpful?
What can we do to improve the information ?