Technical FAQs

Ask a Question

The ATV58HU18M2( V3.1) will operate and run normally. However, the ATV58HU18M2 will display "nst" when VW3A58310 Ethernet card is installed on it. We...

Goals and Symptoms

The ATV58HU18M2( V3.1) will operate and run normally. However, the ATV58HU18M2 will display "nst" when VW3A58310 Ethernet card is installed on it. We have confirmed there has no "freewheel" or "fast stop" is assigned to I/O. How to solve this problem from "nst" to "rdy" in order to operate the ATV58 by AI1when Ethernet card is installed?

Causes and Fixes

In fact this function ( Forced local mode ) is not directly possible with the ATV-58 on V3.1 ( corrected on V4.xx ) but avalaible on the 58F.

To solve it, use the Web server ( information on page 48 §8.6.3 from the Ethernet card user manual ). Replace your 58 by 58F or waiting November for V4.xx.



 


Legacy KB System (APS) Data: RESL156488 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?