Technical FAQs

Ask a Question

Some of the values for the parameters are not visible. All that is displayed is *. What could be causing this. I am attaching a screen capture and the...

Goals and Symptoms

Some of the values for the parameters are not visible. All that is displayed is *. What could be causing this. I am attaching a screen capture and the file for you information.

Facts and Changes

ATV68, Powersuite V1.5

Causes and Fixes

The problem come from your PC configuration, is in Irish english; change it to International english or American english.


Legacy KB System (APS) Data: RESL156487 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 68
Was this helpful?
What can we do to improve the information ?