Technical FAQs

Ask a Question

1. The wiring method of Modbus car / LonWorks module. How to connect with twisted pair cable w/o connector ? 2. Display parameters of VVD :- P-P or P...

Goals and Symptoms

1. The wiring method of Modbus car / LonWorks module. How to connect with twisted pair cable w/o connector ?
2. Display parameters of VVD :- P-P or P-N output voltage show ? 3 the power consumed shown is motor power or VVD power ?
4 the running hours shown is accumlated or reset after power off ?

Facts and Changes

Drives are used in Building for HVAC application

Causes and Fixes

1- it's not possible the gateway w/o connector, one RJ45 for the modbus slave and one 5 terminals ( screw ) for the Lonworks.

2 - What do you mean by - P-P or P-N output voltage show ?
3 - APH, power consumed is for the motor
4 - The running hours ( RPR ) is accumulated but you need v5.2 ie37 control board to reset it and only for the inverter.


Legacy KB System (APS) Data: RESL156450 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38
Was this helpful?
What can we do to improve the information ?