Technical FAQs

Ask a Question

Cannot connect to ATV58 Web Server with Internet Explorer

Cannot connect using Internet Explorer (IE) to the embedded webserver of two ethernet cards VW3A58310 of an ATV58

Altivar 58 VFD
VW3A58310 embedded ethernet cards

IP addresses must be set and exist on the same subdomain to enable communication.

1.    Verify the IP address is set correctly.
2.    Check the wiring by pinging the IP address of the cards.
3.    Remember there is a maximum of 8 connections at the same time.
Was this helpful?
What can we do to improve the information ?