Technical FAQs

Ask a Question

I need to find the part number for the current sensor (CT) mounting braket for the ATV66 size 7. There was an information sheet sent out some years a...

Goals and Symptoms

I need to find the part number for the current sensor (CT) mounting braket for the ATV66 size 7.
There was an information sheet sent out some years ago directing that the steel mounting brackets be replaced with alloy brackets.
I believe these alloy brackets were given a part number but I have lost the information and was hoping you could help.
Can you please supply me with the part number.

Facts and Changes

ATV66

Causes and Fixes

The maintenance manual is in Attachments.

ATV66C10N4 = VY1A66106
ATV66C13N4 = VY1A66106
ATV66C15N4 = VY1A66107
ATV66C19N4 = VY1A66107

Was this helpful?
What can we do to improve the information ?