Technical FAQs

Ask a Question

Some of the values for the parameters are not visible. All that is displayed is *. What could be causing this. I am attaching a screen capture and the...

Goals and Symptoms

Some of the values for the parameters are not visible. All that is displayed is *. What could be causing this. I am attaching a screen capture and the file for you information.

Facts and Changes

ATV68, Powersuite V1.5

Causes and Fixes

The signification of the " * " is:

parameter modified, different to the factory setting.

In your case you modify your PC configuration to international or american english, not irish.

Was this helpful?
What can we do to improve the information ?