Technical FAQs

Ask a Question

WHAT IS THE VALUE OF THE POWER DISSIPATED BY ATV11HU05M2E ?

Goals and Symptoms

WHAT IS THE VALUE OF THE POWER DISSIPATED BY ATV11HU05M2E ?

Causes and Fixes

ATV11 Europe 4 Khz

Loss :

0,18 kW 9W
0,37 kW 17,6W
0,55 kW 26W
0,75 kW 33,6W
1,5 kW 68,4W
2,2 kW 92,6W

Add 5 W for the control board


Legacy KB System (APS) Data: RESL156391 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 11
Was this helpful?
What can we do to improve the information ?