Technical FAQs

Ask a Question

We have 2 x motors (1 duty , 1 standby), 2 x VSD (1 each motor) and 1 x 11kW fan Both duty and standby are connected to the fan by seperate V belts, t...

Goals and Symptoms

We have 2 x motors (1 duty , 1 standby), 2 x VSD (1 each motor) and 1 x 11kW fan Both duty and standby are connected to the fan by seperate V belts, the standby is just freewheeling. When we transfer duty to standby should we anticipate any problems?

Causes and Fixes

No problem if you active the catch and fly function


Legacy KB System (APS) Data: RESL156389 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 38
Was this helpful?
What can we do to improve the information ?