Technical FAQs

Ask a Question

Why can't I communicate from a PLC on the Modbus Plus network through a BM85 mux, to a PLC on the Modbus port of the BM85?

One reason may be the way the port is configured in the BM85, check to be sure the port is configured as a slave and not a master.


Legacy KB System (APS) Data: RESL156366 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?