Technical FAQs

Ask a Question

Could 110V motor be started with LH4N1___LU7 from the 110V single phase commercial power supply?

Goals and Symptoms

Could 110V motor be started with LH4N1___LU7 from the 110V single phase commercial power supply?

Facts and Changes

LH4N1____LU7

Causes and Fixes

It's possible to supply the product directly under 110 V, you can put an elevator transformer before the LH4 ( on phases 1 and 3 ) and another transformer after the LH4 to reduce the voltage because the motor is 110 V.
Other possibility is to realize a specification but depend to your quantity.
We can also propose you a field test with the ATS01 if the rated current is 3, 6 , or 12 A.


Legacy KB System (APS) Data: RESL156324 V3.0, Originally authored by on , Last Edited by on
Related ranges: LH7, LH4
Was this helpful?
What can we do to improve the information ?