Technical FAQs

Ask a Question

We have an enquiry from a customer for an ATV68E with 48VAC controls. Can this be done? Can the ATV68 control card take 48VAC as an input direct or ...

Goals and Symptoms

We have an enquiry from a customer for an ATV68E with 48VAC controls.
Can this be done?
Can the ATV68 control card take 48VAC as an input direct or is it only 24VDC?

Facts and Changes

ATV68E
48VAC controls

Causes and Fixes

Unfortunatelly it's not possible to supply the control card under 48VAC, it's only 24Vdc and also for the inputs.


Legacy KB System (APS) Data: RESL156322 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 68
Was this helpful?
What can we do to improve the information ?