Technical FAQs

Ask a Question

ATV66 with two motors and two Parameter sets.

Goals and Symptoms

ATV66 with two motors and two Parameter sets.

Facts and Changes

This option doesn't appear in the Display menu, but they are described in the programming manual (VVG307GB)page 50.

Causes and Fixes

There is no particular incompatibility with this functionnality, check if you have a total access to the inverter.


Legacy KB System (APS) Data: RESL156319 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 66
Was this helpful?
What can we do to improve the information ?