Technical FAQs

Ask a Question

ATV68C13N4 central board has failed. This is the second one to fail in 1 week. The VSD was powered up but NOT running. The cooling fans stopeed and th...

Goals and Symptoms

ATV68C13N4 central board has failed. This is the second one to fail in 1 week. The VSD was powered up but NOT running. The cooling fans stopeed and the display went blank.

Facts and Changes

ATV68C13N4

Causes and Fixes

We have had quality problems with some diodes on this case ( they were put in short circuit ), the stock in Evreus has been replace in beginning of June.


Legacy KB System (APS) Data: RESL156315 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 68
Was this helpful?
What can we do to improve the information ?