Technical FAQs

Ask a Question

The menu 8-Communication doesn' t appear on the display and so it is not possible assign an IP address to the ATV. The display shows a menu 8 called A...

Goals and Symptoms

The menu 8-Communication doesn' t appear on the display and so it is not possible assign an IP address to the ATV. The display shows a menu 8 called Application but I don' t know how to use it. Using an ethernet card VW3A58310 v1.1 IE 12 all works fine. Is it possible update the firmware of ethernet card in some way ?

Facts and Changes

ATV58 V5.1 IE 32 Display keypad VW3A58101 V4.1 IE 13 VW3A58310 V1.0 IE 11

Causes and Fixes

Try to replace the keypad by a new one V5.2 ie32, an incompatibility with your control board is possible.
A new version of Ethernet card is forecast for September 2003, waiting that it's possible to update the firmware ( v2.1 ) here for firld test.


Legacy KB System (APS) Data: RESL156311 V3.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?