Technical FAQs

Ask a Question

What is the difference between the 3220 motion controller part numbers 100-037 and 100-037-252?

Both of these parts are CPU I/O boards for a model 3220 motion controller, the 100-037 is a replacement for the 100-037-252. The -252 is a layered board designed for high noise applications.


Legacy KB System (APS) Data: RESL156292 V1.0, Originally authored by on , Last Edited by on
Related ranges: Other Motion controllers
Was this helpful?
What can we do to improve the information ?