Technical FAQs

Ask a Question

What is the difference between the Cyberline 110- 090, -091, -092, -093, and -094 drives?

The CL 1000, 110-09x drives have different motor current classes as follows :

CL 1000 Drive
Current Rating
110-090
5 AMP
110-091
10 AMP
110-092
20 AMP
110-093
30 AMP
110-094
60 AMP

Legacy KB System (APS) Data: RESL156286 V1.0, Originally authored by on , Last Edited by on
Related ranges: Other Motion controllers
Was this helpful?
What can we do to improve the information ?