Technical FAQs

Ask a Question

What causes the "invalid configuration: Company ID is invalid" error when trying to download an application to a Panelmate?

The "invalid configuration: Company ID invalid" error when trying to download a application to a Panelmate is caused due to a software incompatibility between the Panelmate and the Panelmate Configuration software being used. Modicon Plus series Panelmates are only compatible with Modicon Panelmate software. IDT EATON Power series Panelmates are only compatible with IDT Eaton software. If a user attempts to mismatch the software to the hardware, this error occurs. The Company ID is displayed on the system page which is accessible in a Panelmate while in Off-Line mode.


Legacy KB System (APS) Data: RESL156283 V1.0, Originally authored by on , Last Edited by on
Related ranges: Panelmate
Was this helpful?
What can we do to improve the information ?