Technical FAQs

Ask a Question

What are the Twido TWDXPCRTC Real Time Clock option adapter specifications?

The below chart is for the Twido TWDXCPRTC Real Time Clock specifications.

ACCURACY
30 s/month (typical) at 25 DEG C (77 deg.F)
Backup duration Approximately 30 days (typical) at 25 Deg. C (77 deg.F) after backup battery fully charged.
Battery Lithium secondary battery
Charging time Approximately 10 hours for charging from 0% to 90% of full charge
Replaceable Can Not replace battery

Legacy KB System (APS) Data: RESL1552 V3.0, Originally authored by RiTa on 06/15/2012, Last Edited by BrWa on 06/15/2012
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?