Technical FAQs

Ask a Question

Can I install a 140NOEXXXXX Ethernet Card in a Remote I/O drop?

No. All Quantum 140NOEXXXXX Ethernet modules must be be installed in the local rack with the CPU. They cannot be installed in a RIO drop.


Legacy KB System (APS) Data: RESL155004 V1.0, Originally authored by on , Last Edited by on
Related ranges: ConneXium - Ethernet
Was this helpful?
What can we do to improve the information ?