Technical FAQs

Ask a Question

Can the operator change the password in a Magelis terminal while the terminal is running the application ?

No. The passwords are developed with the application and downloaded to the Magelis. If a change to the password is required it must be done in the XBTL1000 software and the application redownloded to the Magelis terminal.


Legacy KB System (APS) Data: RESL154972 V1.0, Originally authored by on , Last Edited by on
Related ranges: Magelis XBT-L
Was this helpful?
What can we do to improve the information ?