Technical FAQs

Ask a Question

l have a question , in the VSD catalogues there is a clause under 'Conformity to standard' EN61800-3 , is there any different using EN61000-6-4 and EN...

Goals and Symptoms

l have a question , in the VSD catalogues there is a clause under 'Conformity to standard' EN61800-3 , is there any different using EN61000-6-4 and EN61000-6-2 standard . If yes , what is the differents ?

Causes and Fixes

IEC61000 is a generic norm and IEC61800 is for starter and inverter and it include the IEC61000

IEC 61000-6-2 Janvier 1999 (36 pages )

Electromagnetic compatibility (EMC) - Part 6-2: Generic standards - Immunity for industrial environments

IEC 61000-6-4 Janvier 1997 (17 pages )

Electromagnetic compatibility (EMC) - Part 6: Generic standards - Section 4: Emission standard for industrial environments

IEC 61800-3 Juin 1996 (171 pages )

Adjustable speed electrical power drive systems - Part 3: EMC product standard including specific test methods

Was this helpful?
What can we do to improve the information ?