Technical FAQs

Ask a Question

Our future costumer is habituated to apply SIEMENS Drives, model Micromaster wich has a JOG button on frontal display, and according of them related, ...

Goals and Symptoms

Our future costumer is habituated to apply SIEMENS Drives, model Micromaster wich has a JOG button on frontal display, and according of them related, this button is permanent able in wiring configuration or keypad command at the same time. I don't known about that, but he asks us if our PRODUCTS are able to work on this way. I did this test in our service laboratory and when I preset wiring mode using logic input for the jog is OK, but when I preset keypad command, it locks the wiring command and the jog operation dont work anymore. There is a way to work ?

Causes and Fixes

With the ATV58 it's not possible to have both command ( ie keypad and wiring ), only one on twice. But it's available with ATV68, depend to the size needed.


Legacy KB System (APS) Data: RESL154936 V4.0, Originally authored by on , Last Edited by on
Related ranges: Other VVD PRODUCTS
Was this helpful?
What can we do to improve the information ?