Technical FAQs

Ask a Question

Many customers use brake resister with ATV58. Can you tell me the DC voltage when the brake begin? And how large brake current(DC) can ATV58 sustain c...

Goals and Symptoms

Many customers use brake resister with ATV58. Can you tell me the DC voltage when the brake begin? And how large brake current(DC) can ATV58 sustain continuously?

Causes and Fixes

The braking transistor is started at:

800 V ( DC bus ) for 400/500V ATV58 range
395 V ( DC bus ) for 200/240V ATV58 range


Legacy KB System (APS) Data: RESL154896 V5.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 58
Was this helpful?
What can we do to improve the information ?