Technical FAQs

Ask a Question

What is the resolution of the AS-BADU-214 analog input?

When using the E984-258/265/275/285 PLC models, only 15 Bit + sign resolution is supported by the AS-BADU-214.
The 12, 13, and 15 Bit + sign resolutions are supported when using the A984-1xx, E984-24x/251/255 PLC models.


Legacy KB System (APS) Data: RESL152 V1.0, Originally authored by on , Last Edited by on
Related ranges: Compact
Was this helpful?
What can we do to improve the information ?