Technical FAQs

Ask a Question

Does the Quantum Hot Standby support Symax I/O?

Yes, Symax Remote I/O will operate in a Quantum Hot Standby system. To connect the Symax I/O to the Quantum RI/O network a CRM931 Remote I/O interface is required and the I/O must be configured in the Application I/O map.
NOTE: All 8030 RIM125 must be updated to 8030 RIM125S if used in current loop mode.
Hold up time default is 3 ms and must be changed to 4 ms.


Legacy KB System (APS) Data: RESL1470 V1.0, Originally authored by on , Last Edited by on
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?