Technical FAQs

Ask a Question

What does Concept error 1316 mean and how can I correct it?

Concept error 1316 is described as 'EFB Type Was Not Installed Previously'. To correct this, verify that all needed EFBs are present in the Concept\LIB folder. Also, close Concept and delete the ~aitmp files in the \LIB folder.

Legacy KB System (APS) Data: RESL1448 V2.0, Originally authored by RoAl on 12/12/2012, Last Edited by DaSo on 12/12/2012
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?