Technical FAQs

Ask a Question

How do I put the Panelmate 1000 into "Transfer Mode" so I can download the program to it?

To put the Panelmate 1000 into "Transfer" mode, you must hold the <Cancel> key on the front of the unit when you apply power to it. This will force the Panelmate 1000 into "Offline" mode after power up diagnostics are completed. You then simply select "Enter Transfer Mode" and press the control button labelled "Execute".

Was this helpful?
What can we do to improve the information ?