Technical FAQs

Ask a Question

Can I extend the working distance of the TER port on TSX Premium and TSX Micro controllers?

Yes, the length of the bus can be increased from 10m to 1000m by using the TSXPACC01 Tap link.


Legacy KB System (APS) Data: RESL1437 V2.0, Originally authored by on , Last Edited by on
Related ranges: Uni-Telway
Was this helpful?
What can we do to improve the information ?